2/12/2010 11:20 AM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi, there is no need for you to buy SmartAccess, SmartService is sufficient. |
mfG / Best regards |
|
2/12/2010 11:35 AM | |
Joined: 4/24/2006 Last visit: 5/17/2024 Posts: 8649 Rating: (1151)
|
Dear Cristi01, Perhaps this link might help: What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the internet (WAN)? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
2/15/2010 9:07 AM | |
Joined: 4/24/2006 Last visit: 5/17/2024 Posts: 8649 Rating: (1151)
|
Dear Cristi01, The answer is NO. WinCC flexible/Sm@rtService is an option to WinCC flexible. You can do the following: - Use Teleservice software, Step 7 and modem at officeandon location a TS adapter II (with integrated modem) to connect to MPI or Profibus. - Use Teleservice software, Step 7 and modem at office and on location a TS adapter IE (With integrated modem) to connect to Ethernet. - Or you can use a VPN tunnel: What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the internet? Best regards, Wizard |
2/15/2010 11:03 AM | |
Posts: 12 Rating: (0) |
Thank you Wizard |