6/11/2012 2:37 PM | |
Posts: 3037 Rating:
|
Hello, I found following FAQ. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Have youenabled on the PC/PG interface the option "PC/PG is the only master on the bus"? Tweety |
6/14/2012 10:55 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello Acorn93, You should perform an OS update with the option "Reset to factory settings" selected. how do you do an operating system update (OS update) on operator panels? also have a look here: What transfer options are available in the various operator panels? it looks you need RS232/PPI multimaster cable or USB/PPI multimaster cable. Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on