1/17/2009 9:26 PM | |
Posts: 14 Rating: (0) |
Hi Jaapie, Thanks for the response. I assume it is possible to use the vbscript too? Do you know example syntax for that as well? Thanks much! Kristie |
1/19/2009 12:39 PM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Also a solution! |
1/19/2009 8:16 PM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Nice, thanks! |
1/21/2009 7:53 AM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Hi Kristie, It does not matter you do not know much of WinCC, that is what we are here for. In a few months you can help too. If I got time I can help.......so Sorry, but if you set the Tagprefix, there is no other way when using tags. In this case I usually create 2 picturewindows for a popup (picturewindow in picturewindow) The first picturewindow (main) is not using a tagprefix the second picture window (within the main) is using the tagprefix. The items you do not want to give a prefix to you can put in the main (e.g autorisation bits or something like that)and all others (with a prifix) you can put in de sub-window. Also this below optioncan give you aidea to solve the problem, I think it will work in your case too but I have never tried: /tf/WW/en/Posts/25490 Hope this gives you an idea. Good luck, Jaap |
This contribution was helpful to1 thankful Users |
Follow us on