Industry Online Support
Technical Forum
9/16/2014 9:29 AM | |
Joined: 9/12/2007 Last visit: 8/24/2020 Posts: 12 Rating: (0) |
Hello, I've installed WinCC option - Information Server 2013 on a WinCC station. However, while installing the software component SQL Server 2008R2 SP1 IS-Server/PH-Server, error received and not installed successfully. I've read through the installation requirements and I am sure the requirements are met. (See attachments) The system bypass this SQL installation and carried out others. I attempted to import archived data in Excel but failed to do so. All the IS Add-in buttons are disabled and keep on prompting for user name & password. I used the same username & password created in Windows and WinCC but to no avail. Meanwhile, I access Info Server using Internet Explorer. But no selection of the WinCC project is available as well. (See attachment) - OS: Windows 7 Professional SP1 (64-bit) - WinCC: V7.2 + Update 6 - MS Office: 2010 SP1 I hope I can receive some guidance on this. Thank you. AttachmentF:\Info Server\16Sept2014\16Sept2014.zip (183 Downloads) |
Follow us on