12/20/2011 8:47 AM | |
Posts: 1776 Rating: (95)
|
Hi, modbus serial driver is not in the WinCC standard delivery. But the driver is available from an other vendor. See FAQ http://support.automation.siemens.com/WW/view/de/21915573 Modbus TCP/IP is included the basic package of WinCC. See WinCC information Manual for Modbus or |
11/22/2016 12:33 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by TienLuongJS123 is split to a separate thread with the subject Can't find Modbus library in my Tia portal. Best regards |
Follow us on