4/27/2016 5:13 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello Pl see the discussions in the following threads on same topic : wincc 7.0 sp3 deactivation problem WinCC 7.0 sp2 Deactivate stop at 35%, help me. TagLogging Runtime ERROR in WinCC 7 Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
4/27/2016 12:48 PM | |
Joined: 3/14/2008 Last visit: 7/15/2024 Posts: 2077 Rating:
|
Hello, There are several programs called by WinCC when activating runtime. You can find them under the OS project->WinCC explorer->Computer and then right click the computername on the right. You have reached the Computer properties and when you go to tab: "Startup" you will see a list of startup items. You can try to enable only: "Graphics runtime". When you can shutdown runtime, you enable Alarm logging, test again and then Scripting. etc.etc. If there are problems with the Scripting, you can use the following program: apdiagnose.exe. It's found under Program Files(x86)->Siemens->WinCC->utools. When in runtime, you can call the program and set the output window open. Now, all scripts running with problems will be presented on the output window. You may report back if there are issues. (Make sure you do this on your OS server(s). You can also upload the following diagnose files found under Program Files(x86)->Siemens->WinCC->Diagnose: - WinCC_Sys_01 - PMDeactivate - PMDiagnose |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
4/27/2016 1:04 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating:
|
Hi, have a look at this FAQ Regards |
4/27/2016 7:45 PM | |
Joined: 4/17/2016 Last visit: 7/8/2019 Posts: 48 Rating:
|
Thank you all, After reorganize the program....problem solved. |
This contribution was helpful to
1 thankful Users |
8/17/2018 12:22 PM | |
Joined: 3/2/2018 Last visit: 6/7/2024 Posts: 3 Rating:
|
Good day, could you explain a little on how you reorganized the project? I am facing a similar problem. |
8/17/2018 8:46 PM | |
Joined: 9/9/2015 Last visit: 7/16/2024 Posts: 727 Rating:
|
Dear Northern Guy, To reorganise project, go to File, Save As, choose the slow reorganize project. But before you reorganise, make sure you did all the necessary back up and archive first. If you have process historian, better not to reorganize your project. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/21/2018 11:27 AM | |
Posts: 64 Rating:
|
What happens when a project with process historian is reorganized? |
Follow us on