5/9/2022 2:15 PM | |
Joined: 6/23/2013 Last visit: 8/1/2024 Posts: 62 Rating:
|
WinCC OA supports the H-PLC, but no redconnect for the S7-400H. The open architecture could be advantage if customization is needed or the same objects can be used many times. It can be modified from the look and feel not only for the end-users, but also the engineering tools. Interfacing with other systems should be easier with WinCC OA. See also an older topic:Is WinCC OA the "better", the modern alternative / successor of WinCC V7? |
WinCC OA expert |
|
Follow us on