6/23/2009 11:25 AM | |
Posts: 35 Rating: (0) |
it is possible, you can use Web Navigator. You can read about it in Wincc Contents underOptions. |
6/23/2009 11:35 AM | |
Posts: 49 Rating: (18) |
Hi, If i understand it correctly, you have two OS station in standalone mode, distance between two of them is 3KM. Basically distance between two standalone stations wont be a issue at all, as both the station have to communicate to one AS system. in that case you may have to use a MEDIA CONVERTORi.e.something which shall convert physical medium from Ethernet to Fibre Optic andvice versa. please find attached Example for the same. note: Please use the attached file to match specifications only. you can use any local device. so now, your AS toWinCC station Physical path would be AS >> Ethernet Switch >> Media convertor 1 >> LIU >> FO Cable >> LIU >> Media convertor 2 >> Ethrenet switch (optional) >> WinCC station. LIU = :Light InterfaceUnit i.e. Passive device for coupling. Easily availabel in market. But please note that, Still your PROTOCOL for communication would be ETHERNET only. regards, Enigma AttachmentMedia convertor.pdf (69 Downloads) |
6/23/2009 12:44 PM | |
Posts: 133 Rating: (9) |
Yes Enigma is correct Good luck with the implimentation. |
6/24/2009 11:58 AM | |
Posts: 16 Rating: (0) |
Hi Enigma, Thanks for your solution about Web navigator. Is it possible to go for "TELECONTROL(teleservice over telephone line)", here i am attaching catalog for your information. kindly go through it and suggest your view on this. Regards, Sunil AttachmentTelecontrol.pdf (95 Downloads) |
Follow us on