9/21/2016 3:43 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
Hello Milosh, here is a list of all the properties and methods of the "Table view" control in VBS: (It's a link to the V13 SP1 WinCC Professional manual because the V12 SP1 one didn't open properly... but this particular content should be the same, I think.) Maybe there is something in the list that helps you. I don't work with protocols, so I can't give you any advice on that front. On another note: maybe the following application example could be some kind of solution to your Problem. But it's made in WinCC Advanced and I don't know it it's fully adaptable to WinCc Professional. Some changes at least would be necessary (different control = different vbs functions).
|
Last edited by: H.J. at: 9/21/2016 3:48:42 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on