6/5/2019 11:44 AM | |
Joined: 9/9/2013 Last visit: 7/3/2024 Posts: 11 Rating: (0) |
We are running a WinCC 15.1 Runtime Advanced application on a panel-PC. After running the software for a while, an dialogue is displayed with the following message message: Despite the error message the application seems to be working fine, but the dialogue is rather annoying and our customer will not accept the system as it is. Note: A similar case can be found here: https://support.industry.siemens.com/tf/ww/en/posts/wincc-runtime-advanced-v15-error/190552. That problem was solved by updating Automation License Manager (ALM). We have tried the following: Any ideas? Are there any log files that can be checked for more information on what is generating the message? System data:
|
7/25/2019 1:55 PM | |
Joined: 8/3/2009 Last visit: 7/19/2024 Posts: 13341 Rating: (1692)
|
Hello I would try to deinstall the ALM restart the PC and install the one you can download from the Support Pages: https://support.industry.siemens.com/cs/de/en/view/114358 this helps us in the past Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on