1/27/2014 2:54 PM | |
Posts: 7 Rating: (0) |
Hi, I am having problems connecting my WinCC RT advanced to a 1200 plc. When i create an HMI PC station and use an IE general for connection, I connect it to the same PN/IE connection between the PLC and the PC Station. It gives me an error when i select the tags for the PLC address in the GUI setup. If i setup a SEIMATIC TP1500 or any other HMI panel the PLC tags are automatically imported for use in the GUI. This doesnot happens when i try to setup WinCC RT Advanced to connect to the PLC i get invalid internal tag. If i try to make the connection myself it gives me errors. Any help would be appreciated. I have read up on other threads here and they were not helpful with regards to this problem. I have uploaded screenshots.
AttachmentScreenshots.zip (538 Downloads) |
Last edited by: tx1000 at: 1/27/2014 3:24 PM |
|
2/4/2014 3:32 PM | |
Posts: 7 Rating: (0) |
Hi! I tried the procedure that you outlined and i get error saying that a connection cannot be established with the PLC. I have attached screen caps. I see that when i add a comfort panel HMI and create a screen in that it works perfectly when i use the simulation. The connection is also automatically added to the HMI portion. The network address are in the same subnet and the pc name and ip is the same as well. Is there a step i am missing? Thanks AttachmentScreen Cap.zip (381 Downloads) |
2/4/2014 4:29 PM | |
Posts: 7 Rating: (0) |
Hi K!ke ! I have attached the new screen caps. There are no connections in the HMI connections tag. AttachmentSCADA Screen Cap.zip (371 Downloads) |
2/5/2014 1:26 PM | |
Joined: 9/14/2012 Last visit: 4/25/2024 Posts: 87 Rating: (12) |
1.IE Genral Version(example V7.1 orV 8.1) 2. Your PC system IPandProject IP are Same(192.168.0.2 example) currently i dont have TIA V11. am using TIA V12 so i cant attach sample project .I am attachedstep by step . Screen shots for your info. AttachmentS7 1200 WITH WINCC RUNTIME ADVANCE COMMUNICATION.zip (808 Downloads) |
Regards, |
|
This contribution was helpful to4 thankful Users |
Follow us on