4/1/2020 8:36 PM | |
Posts: 2 Rating: (0) |
Hi, It seems difficult to get working Tag indirect addressing with symbolic access in the WinCC RT Professional v14. (See the attached picture Snap12 - WinCC professional; indirect addressing with symbolic access in the zip-file). It works fine with WinCC advanced. (See the attached picture Snap7 - HMI; indirect addressing with symbolic access in the zip-file) Do You have any solutions on this topic? I don't want to have the answer use UDT, structure or prefix because it's not working with project in the PLC. Attachmentindirect addressing.zip (138 Downloads) |
4/20/2020 1:12 PM | |
Posts: 2 Rating: (0) |
Hi, Thank you Murof for the answer and the solution on this topic. |
Follow us on