10/14/2013 10:20 AM | |
Posts: 4 Rating:
|
My last question is : how can I load WinnCC directly in runtime modewhen Ipower upthe computer, without the need to open WinCC Explorer ? Thanks ! |
10/14/2013 11:55 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating:
|
Hello minorex, When you boot the computer you want to have a specific project started in the WinCC Control Center or in WinCC Runtime depending on the user logged in. If you are using the "AutoStartRT.exe" program, it is only possible to start WinCC directly when the computer is booted independent of the user logged in (see "WinCC Information System > Working with WinCC > Working with projects > Activate project > How to set up the Autostart"). |
Ammy |
|
This contribution was helpful to
1 thankful Users |
7/13/2020 10:36 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating:
|
New question published by PCR092104 is split to a separate thread with the subject BSOD error message 0x00000050(STOP) . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on