2/3/2010 2:28 PM | |
Posts: 9 Rating: (2) |
Hi, I have a problem when activating my runtime (I use WinCC 7.0 SP1 & HF4). I start the runtime in WinCC exporer, I see the progress like normal, and then the runtime starts, but I don't see any screen ... the only thing I see is still the WinCC explorer. I also see that runtime is activated ... but no visual of the startscreen. When I open a screen in graphics designer, and activate that screen, runtime works like normal, I see the screen. I attached some files from diagnose for help. Thanks in advance. Attachmentdiagnose.zip (509 Downloads) |
2/4/2010 4:13 PM | |
Posts: 9 Rating: (2) |
Hi, the checkbox is certainly checked, no doubt about that. but when I activate runtime, I now see that It doesn't get to 'graphics runtime' in the popup loading screen. when i restart my pc, sometimes it works, sometimes it does not. I attached the new zip-file with files from wincc diagnose. Attachmentdiagnose.zip (327 Downloads) |
Last edited by: Bubs at: 2/4/2010 4:17 PM |
|
Follow us on