6/9/2006 3:16 AM | |
Posts: 13 Rating: (1) |
Hi I have a multi-user application. I have added the client machine on the "computer" tag, created an appropiate package and defined an user with "Activate remote" and "Configure Remote" options. Both client and server machines are on the same network and login with the same window count. I'm using win2k sp4 in both of them. I can see each PC from the other. I have the project open and running on the server. In these conditions I try to open the same project from the client. A system login window appears, so i enter the created user. It seema that wincc recognizes it. But then the following message appears: "The \\g2server\\wincc60_proyect_spenceprj\spenceprj.mcp file could not be loaded" and I can't load the project. The same error happens with the project not running on the server. Also I used the autostart option to open it from the server. The system login window appears and the user is accepted, but the following error appears: "Error while activating the project \\\\g2server\\wincc60_proyect_spenceprj\spenceprj.mcp. Autostart not possible" I can't open the Simatic Shell from Windows Explorer, but i can open it from the open project window in wincc. I don't know if this is related to my problem. I hope you can give some advise. Greetings |
6/9/2006 3:18 AM | |
Posts: 13 Rating: (1) |
Sorry, i forgot to say that i can open this project from the client when the server is loading another project, but that is not of much help to me. |
6/9/2006 8:55 AM | |
Posts: 3149 Rating: (171)
|
Hi, please check these FAQ: http://support.automation.siemens.com/WW/view/en/1014417 http://support.automation.siemens.com/WW/view/en/16754155 nemo |
6/12/2006 10:04 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
In response to your points: |
6/14/2006 9:13 AM | |
Posts: 1084 Rating: (72)
|
Hi, Forgot how to calculate the needed subnetmask at the moment, but shouldn't the subnet be set to 255.255.255.0 ? with regards, Ikkezelf |
Follow us on