12/30/2019 7:37 AM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hello Georg Berghof, Thank you for the replay, I little bit confused with the Simatic Audit installation. I don't think my server and clients having Audit installation. Anyway, kindly look at the installed software list available on the attached image, One more information to you, If Wincc update is necessary as you mentioned, then why do my clients not having this issue? My client PC's not creating such errors with the same Wincc versions. Looking forward to your response... AttachmentOSSVR_INSTSL.SW.zip (94 Downloads) |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on