3/10/2009 8:55 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, I suggest you to look at SIMATIC HMI WinCC flexible 2008 Runtime (from page 15). There you'll see how the process visualization software WinCC flexible Runtime is used to run the user program regards |
3/10/2009 11:34 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Well, no your "route" is not possible. But oposite is possible. Look at How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing? plus How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? .In this links you can find also information about which modules possess routing capability. regards |
3/10/2009 12:44 PM | |
Posts: 3 Rating: (0) |
ok i will take a look, and many thanks again :) |
Follow us on