10/2/2024 11:36 AM | |
Joined: 12/6/2023 Last visit: 10/3/2024 Posts: 3 Rating: (0) |
After installing one of the following versions: - TIA 19 - TIA 17 update 8 I have several problems in the software compilation of the operator panels on TIA 14. Depending on the panel being used, different errors come out (attached photos). In particular, these panels give problems: - KTP400 and KTP700 - MP277 - TP2200 The only panel that seems to give no problems is TP1200. Tried both repairing and reinstalling TIA 14 but nothing changes. Uninstalling versions of TIA 17 update 8 or TIA 19, the error continues to persist. The only way to fix it is to return the machine to the state before installing TIA 17 update 8 or TIA 19. Does anyone have any advice for me? AttachmentErrors.zip (49 Downloads) |
10/3/2024 8:40 AM | |
Joined: 8/6/2018 Last visit: 11/6/2024 Posts: 297 Rating: (40) |
Hello, Could you please send us the screenshot of the errors in English? Thanks you |
Follow us on