5/12/2014 8:54 AM | |
Posts: 1299 Rating: (136)
|
Hello, you can use screen windows K!ke |
5/12/2014 12:03 PM | |
Posts: 5225 Rating: (1192) |
Hi-ya, Please look at the attached example that works under WinCC V11 using a BASIC panel. It simulates a full page popup and returns back to where it came from. The PLC determines which page apears as popup. Please review in detail the variables used and what properties were set. I am unsure to what you need the popup for and how you wish to use it. This is the best guess I can make. There are other alternatives: * Make a text block visible * Use loop-in-alarm function inside the alarm popup window. You will be sure to receive more answers if you give a bit more detail. Greetings. w AttachmentEXAMPLE_Simulated popup page .zip (292 Downloads) |
5/12/2014 5:14 PM | |
Posts: 165 Rating: (19) |
hi i m using TIA wincc v11 profesional |
5/12/2014 5:16 PM | |
Posts: 165 Rating: (19) |
Dear william please give solution for wincc profesional v 11 sp2. thanks
|
5/14/2014 7:46 AM | |
Posts: 1299 Rating: (136)
|
Hello, see this thread: /tf/WW/en/Posts/67656 K!ke |
Follow us on