7/9/2018 10:57 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Dear user, ################################################################################# Mobile Panel 2nd Generation Mobile Panels 2nd Generation can be configured with TIA Portal V15. However, the compiled project cannot be loaded to these devices.Until further notice, it is recommended to use HMI version 14.0.1.0 in new projects as well as in existing projects.. You can find additional information here: 109753749 ################################################################################# With best regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
This contribution was helpful to1 thankful Users |
Follow us on