Industry Online Support
Technical Forum
11/24/2020 2:46 PM | |
Joined: 11/6/2020 Last visit: 10/17/2024 Posts: 14 Rating: (3) |
I am new to the Unified panels and am trying some things. I tried to create a screen and after that changing the device type. (From a MTP1500 to a MTP700). According to the information about the Unified panels is it easy to switch between different Unified types. (It doesn't matter if it is a MTP1500 or MTP700). After changing the device the screen didn't scale to the new device. Am I doing something wrong, is this functionality not implemented at the moment or are the Unified Panels not as scalable as promised? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2020 08:34:05New subject after splitting |
|
Follow us on