7/23/2023 12:01 PM | |
Joined: 7/9/2011 Last visit: 6/7/2024 Posts: 19 Rating:
|
Hi, Until two days ago, I didn't have any communication issues. While dealing with another problem related to data export of the trend object, I uninstalled and reinstalled TIA v18, but after that, I couldn't establish the connection. I have made all the necessary settings that I previously did. The errors shown in the Trace Viewer file is attached.. 192.168.0.3 and 192.168.0.11 are online (PLC Sim v18) and the others not. (Previously, it was also like this) PG/PC interface setting is OK. But no connection. Thank you in advance for your assistance. AttachmentTraceViewer.txt (220 Downloads) |
Follow us on