12/27/2019 10:53 AM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424) |
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Recipes (Parameter set) are an important tool for process operation, regarding to transfer and manager machine / plant parameters sets. This sample program shows a simple 3 variables S7-1500 Parameter set been controlled by a WinCC Unified Application Configuration main steps: The main steps are showed in the follow diagram: PLC DataTypes | |---------------- | | V V PLC Tags HMI User Data Type (Project library, types) | | |<-------------| | | V | HMI Tags | | | |<-------------- | V Parameter Set Types | V Parameter Set Object (Screen) The detailed configuration steps are displayed in the Help System, under, Information System, Visualize process, Visualizing processes with WinCC Unified, Configuring Parameters Sets (RT Unified), Creating a parameter set type with elements via a PLC user data type. Project (.zap16 ziped as .zip) AttachmentRecipes2.zip (1634 Downloads) |
Last edited by: Denilson Pegaia at: 12/27/2019 19:23:41Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |
1/19/2024 9:32 AM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424)
|
Hi As from TIA V19, it is possible to use text list and graphic lists in the Parameter Control object. This could make the recipe's operation more clear and to avoid errors. TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentrecipes2_20240103_1634.zip (215 Downloads) |
Last edited by: Jen_Moderator at: 01/19/2024 11:07:54Text formatting optimized. Denilson Pegaia |
|
Follow us on