12/4/2019 5:18 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating: (1438)
|
Hi, As from the TIA V16, there was the introduction of the WinCC Unified. This is an engineering platform for HMI Comfort Unified and for WinCC Unified PC. It brings many news regarding the WinCC Advanced / WinCC Professional. One of these news, is the use of web pages to simulate and debug applications. To enable the IIS features, go to windows' control panel -> programs -> Turn Windows features on or off -> mark: "Internet Information Service" folder, and inside this folder, all suboflders of "Word Web Side Service" / "application development features". The ISS configuration is explained in details in the FAQ Which Windows functions must be activated in order to be able to install SIMATIC WinCC Unified? https://support.industry.siemens.com/cs/ww/en/view/109773589 An secundary topic about web access concerns to certificates. A good guide about it is avaliable in the FAQ How do you create a certificate structure for the WinCC Unified System so that other terminal devices can communicate encrypted with the Runtime? AttachmentPictures.zip (2352 Downloads) |
Last edited by: Denilson Pegaia at: 12/19/2019 11:53:35Last edited by: Denilson Pegaia at: 01/27/2021 11:05:35Denilson Pegaia |
|
This contribution was helpful to34 thankful Users
|
Follow us on