4/30/2024 1:06 PM | |
Joined: 1/21/2013 Last visit: 6/12/2024 Posts: 2877 Rating: (460)
|
Hi AlthanMaiel, I did a test on this topic and ran into the same problem. It seems that the value of the @CurrentLanguage system tag is not passed correctly to the resource list. However, it works if you use an internal HMI tag that carries the same information. So that would be a workaround. However, I would suggest that you create a support request to bring this issue to the attention of the developers. Kind regards |
5/1/2024 4:23 PM | |
Joined: 11/12/2021 Last visit: 5/29/2024 Posts: 5 Rating: (0) |
Thank you really much ! I didn't think about using another tag as a buffer !! |
Follow us on