8/2/2006 10:53 PM | |
Posts: 11 Rating:
|
Hi Nemo, See Attached zip file. The 2 clients that are not working are running W2K SP4. I have 2 more with W2K SP4 and 2 with XP SP1that are working. These 2 also have WinAC on them. (So does 2 others that are working.) Disk space free = 75GB out of 80GB; Virtual Memory free = 700MB out of 768MB; RAM free = 44MB out of 256MB Level 6 I put in the install disk and selected remove wincc completely. I did nothing else. char SQLQuery[254]; char cLine[254]; char cWashCode[254];
//*******Connect to User Archives Component **************************** //*******Connect to Archive via Archive Name **************************** //*******Opens Archive***********************************************
if ( uaArchiveMoveFirst ( hArchive ) == FALSE )
// Set Display Values... SetPropChar(lpszPictureName,"txt_Date","Text", cDateTime);
//******Release Connection to Archive ************************************* //*******Disconnect User Archives Component ************************* return; I am running similar code on the clients in question with the exeption that it is not getting any date time data from the archive. Could this be the problem???? Thanks for your help, Regards Knucklhead Attachmentdiag.zip (527 Downloads) |
Follow us on