4/17/2008 8:40 PM | |
Posts: 6 Rating: (0) |
We have a WinCC station talking to 12 S7-315/317 PLC's over a ethernet network. I got the first eight PLC's to talk but can not get the others to talk. I did install the full Softnet IE as the lean only talks to 8 PLC's. I can ping the bad PLC's and even see them if I create a new WinCC project with the three in it. I get an error code of Errorcode 0xFFDF 4104! but have had no luck finding out what this is. Any help?
Attachmentwincc com.ZIP (247 Downloads) |
Last edited by: Greg R at: 4/23/2008 4:20 PMThanks for all the feedback. I have the correct license files installed. I have tested the application and deleted connections as can be found on the attached spred sheet. No luck. I even di a new application, same problems. The attached zip just has a spread sheet showing test performed and outcomes. Last edited by: Greg R at: 4/18/2008 1:12 PM |
|
4/21/2008 11:23 AM | |
Posts: 1776 Rating: (95)
|
Hi, have you checked the communication resources? See http://support.automation.siemens.com/WW/view/en/299124 Next step to try, remove one of the working PLCs from the PLC list. Can you the communicate with the next bad PLC, so you can communicate always only with 8 PLCs |
4/23/2008 6:31 PM | |
Posts: 6 Rating: (0) |
I tried the steps. No luck. I posted a file of the steps I took and the results. If you get time please take a look. Thanks for the help. |
Follow us on