7/7/2015 4:11 PM | |
Joined: 5/20/2015 Last visit: 8/1/2024 Posts: 216 Rating:
|
hellow all dear. i want to configure a simple PUSH BUTTON application in Wincc explorer v7.0, i refer every manual but not getting success, could anyone guide me STEPWISE that how to do it, i want to configure simple push button application, so that button can make bool bit high while it is press by left mouse key, and get low when it is released, please help, ASAP. ---------------------------------------------------------------------------------------------------- Split from WinCC Explorer Graphic Designer, properties dialog not pop-up. Closed cause question posted twice. The second thread with the subject Push Button application in Wincc V7.0 is published within the conference SIMATIC WinCC.
|
Last edited by: Min_Moderator at: 7/8/2015 10:55:14 AMNew subject after splitting and closed Let's do it... |
|
This contribution was helpful to
1 thankful Users |
Follow us on