6/7/2011 6:39 AM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating: (118) |
Hi, Login as a administrator and try the same and if it is working we can confirm that there is no problem with the installation. or If you get the error only in the user login please see the below attachement for the authorization for the user account in my PC. One more thing, you can check in the services (Run=> Services.msc) for starting of all WinCC related services and if you feel some of the services are not running, you can enable the required services in the msconfig (Run => msconfig) You can check in the SQL database also weather all the services are running as shown in the attachment.
AttachmentDesktop.zip (910 Downloads) |
Last edited by: Saravana kumar at: 6/7/2011 7:06 AMHi, I am really sorry for giving the wrong attachment. Now I have corrected it. Last edited by: Saravana kumar at: 6/7/2011 7:06 AMHi, I am really sorry for giving the wrong attachment. Now I have corrected it. _______________________________________________________________ |
|
6/7/2011 6:48 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, have a look at the following FAQ-Why do you get the message "Open WinCC project: The user does not have the rights to perform this action!"?. http://support.automation.siemens.com/WW/view/en/22780433 |
VANDE MATARAM..... |
|
6/7/2011 7:33 AM | |
Joined: 10/3/2010 Last visit: 6/25/2024 Posts: 1556 Rating: (190) |
Are you trying this with Remote Desktop or locally on the PC? With Remote Desktop, you can also have strange effects if you don't connect to console. |
B r g d s , |
|
6/8/2011 4:03 AM | |
Posts: 4 Rating: (0) |
Simatic Net, PC Software Edition 2008 is installed (along with its Simatic NCM V5.4). The target PC operating system is Win XP Pro SP3. |
6/8/2011 7:00 AM | |
Posts: 487 Rating: (36) |
Talking to some other wincc specialist they also had the problem , they did the same as you to solve the problem .they also contacted Siemens and were told to install the latest update for Wincc V7 SP2 its update 4. Eric |
Follow us on