4/11/2016 10:38 AM | |
Joined: 9/18/2013 Last visit: 2/20/2024 Posts: 203 Rating: (12) |
Hello, You can try to reset WinCC Open: Run Type: reset_wincc.vbs |
4/12/2016 10:21 AM | |
Joined: 10/3/2010 Last visit: 4/25/2024 Posts: 1552 Rating: (188) |
Does this happen on all pdl's or just a single one on that PC? |
B r g d s , |
|
4/12/2016 11:08 AM | |
Joined: 6/28/2007 Last visit: 12/13/2023 Posts: 61 Rating: (4) |
Hi i Guess u have misunderstood the senario. This was a project running in a PC which was in a Windows Domain Configuration, Now i have copied the backup to my PC which is in Workgroup domain There is a strange error that i am recieving in the log file PMDiagonise i have attached kindly look into.. Regards SPV AttachmentPMDiagnose.txt (285 Downloads) |
Best Regards & Thanks in Advance |
|
Follow us on