12/17/2019 1:38 PM | |
Joined: 9/20/2017 Last visit: 3/20/2024 Posts: 27 Rating: (0) |
Hi, I am using wincc v7.4 sp1 and siemens cpu 414-5H PN/DP. i am trying to create redundant connection but unable to create redundant connection. i am using TCP/IP driver for the tags. i have installed step7 simatic manager in the same pc. if it is not possible to do same then suggest a way to create redundant connection for above mentioned system. can i use any other driver in tag management. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/18/2019 09:02:13New subject after splitting |
|
12/23/2019 4:28 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi, Are you using extra licenses as WinCC Redundancy and have this option installed? B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on