2/7/2019 7:42 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2168)
|
Hello HarveyD, if you a generally problem with the installation of WinCC V7.5, you should use the SIMATIC Assessment Suite - Data Collector (SAS-DC) - formerly known as SIMATIC Diagnostics Tool (SDT) - to collect diagnostics and system information from the Computer. https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Service Request an send the data to the Technical Support of Siemens. The channel is in the attachment, I hope it helps. Regards Georg Berghof AttachmentOPC UA WinCC Channel.zip (612 Downloads) |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
Follow us on