2/12/2021 2:14 PM | |
Posts: 13 Rating: (0) |
Schufri, Which file inside the diagnose folder would you want to see? |
2/12/2021 2:37 PM | |
Joined: 10/10/2014 Last visit: 5/17/2024 Posts: 1725 Rating: (209) |
Hi ChrisH_ATL Zip all the files expecting any dump files and post the zip file Best regards schufri |
2/12/2021 2:51 PM | |
Posts: 13 Rating: (0) |
I have uploaded the folder with the removal of license information.
AttachmentRSProject.zip (224 Downloads) |
2/12/2021 3:01 PM | |
Joined: 9/1/2017 Last visit: 5/19/2024 Posts: 156 Rating: (19) |
Hi Which exact edition of windows server 2019 do you use? Please have look at operating system compatibility table. Regards hosein P.s: have you tried resetting archives? |
Last edited by: hosein8419 at: 02/12/2021 15:04:34 |
|
This contribution was helpful to1 thankful Users |
2/12/2021 3:24 PM | |
Posts: 13 Rating: (0) |
Hosein8419, I'm using Server 2019 Standard which is fully supported. |
2/12/2021 3:32 PM | |
Joined: 10/10/2014 Last visit: 5/17/2024 Posts: 1725 Rating: (209) |
Hi Chish_ATL, in the diagnostic files cam's a lot of error message regarding CCDmRtServer and PLC communication Updates for WinCC V7.5 SP1 and WinCC V7.5 SP1 ASIA See CCDmRTServer,log SIMATIC_S7_PROTOCOL_SUITE_01.log SIMATIC_S7-1200_S7-1500_Channel_02.log Best regards |
This contribution was helpful to1 thankful Users |
Follow us on