5/22/2011 2:54 PM | |
Posts: 8946 Rating: (999) |
Oh dear, with SP2: Yes. http://support.automation.siemens.com/WW/view/en/22055368 |
5/22/2011 3:05 PM | |
Posts: 378 Rating: (47) |
Hello, maybe additional info is helpful too. WinCC 7.0 SP2 http://support.automation.siemens.com/WW/view/en/21927773 Best regards Bilao |
5/23/2011 10:31 PM |
|
Posts: 947 Rating: (45) |
And Update 3 for WinCC V7.0 SP2 and WinCC V7.0 SP2 ASIA http://support.automation.siemens.com/WW/view/en/48694762 |
6/9/2011 1:41 PM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating: (31) |
hi, refer atatched doc. viral patel
AttachmentWinCC_V7_compatibility_list_e[1].pdf (469 Downloads) |
4/26/2012 5:34 PM | |
Posts: 8946 Rating: (999) |
What you are saying is completely wrong! |
4/27/2012 7:11 AM | |
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating: (12) |
Hi IBN-Service, As per the compatibility matrix tool, its showing thatWinCC Flexible 2008is compatible with Windows XP SP3. It doesnt give any info about the Windows 7 compatibility. You can refer the attached screenshots AttachmentCompatibility.zip (401 Downloads) |
Regards, |
|
4/27/2012 8:21 AM | |
Posts: 378 Rating: (47) |
Hello RJ, i think you are wrong, because Sarfraz Bhatti wanted to know if he can install WinCC flexible 2008 on Win7 32bit. And the answer is yes, with SP2 or SP3 he can install it. (See attachment) Best regards Bilao |
This contribution was helpful to1 thankful Users |
Follow us on