1/29/2023 6:01 PM | |
Joined: 10/1/2021 Last visit: 6/8/2024 Posts: 22 Rating: (0) |
Dear Experts, I wanted to run a project using Wincc7.4 Sp1 at Wndows server 2016. When i open a new project it is opening successfully after completing software installation, But when i open graphics designer editor i found all tools are not working. I am unable to drag and drop any tools to the editor. Then i close the graphics designer editor. And then when i try to close the WinCC it is continuously hanging. I had to close it forcedly. Note: I was working from remote desktop connection. My questions are 1. Is it compatibility issues between WinCC 7.4sp1 and Windows server 2016? 2. If it compatible how could i solve this issues? 3. Is it installation issues or due to windows server 2016? I look forward to hearing a best solutions from you. Thanks in Advance ------------------------------------------------------------------------------------------ |
Last edited by: JasimUddinJosh at: 01/29/2023 18:02:52Last edited by: The Helping Hand at: 01/31/2023 08:39:55New subject after splitting |
|
Follow us on