5/30/2022 11:47 AM | |
Joined: 8/3/2009 Last visit: 7/15/2024 Posts: 13287 Rating:
|
Hello glato If you are using new PLC FW of V17 and WinCC V7.5 SP2 Upd4 or newer then you only can work with the SCADA Export Tool for the first time to get the certificate fo rthe connection. after that you should also be able to use the online connection if the Runtime is running. Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109798498 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on