Industry Online Support
Technical Forum
9/23/2010 10:36 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello Michele; How have you setup your message archive for alarms? Have you had a look at this manual: Working with WinCC? It is a large download but thecontents are wellworth the trouble. http://support.automation.siemens.com/WW/view/en/37436840 Examinech. 5.5.2.3: "How to configure amessagearchive" and the following paragraphs; it will show how to configure the properties of your alarm archive: For example: Make the following settings for the archive: · Time period of all segments and their maximum size. This specification defines the size of the archive database. If one of the criteria is violated, a new segment is started and the oldest segment is deleted. · The time period in which messages are to be archived in an individual segment and its maximum size. If either of these criteria is violated, a new individual segment is started. When the criterion for "Time period of all segments" is violated, the oldest individual segment is also deleted. In the "Time of the segment change" field, enter the start date and the start time for the first segment change. When a new individual segment begins, the configuration of "Time of the segment change" is taken into account. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/23/2010 10:37 PM |
|
9/24/2010 11:42 AM | |
Posts: 25 Rating: (0) |
Thanks for your support, i have read this document before but maybe i forgot something which you show me detail! thanks alot! |
Follow us on