Industry Online Support
Technical Forum
5/6/2011 9:35 AM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148)
|
Dear smodlaka112233, So you got the message "OS not compatible" (There is connection) Now you have to perform an OS update, see link how do you do an operating system update (OS update) on operator panels? Here are some links about transfer project: how can you transfer a WinCC flexible project serially to a panel? how can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? One important thing: Change the name of panel. (See point 4) Best regards, Wizard |
Follow us on