3/6/2011 9:41 AM | |
Posts: 95 Rating: (1) |
HI all, Splitted from Windows Server 2008 & WinCC. |
Last edited by: O_Moderator at: 3/8/2011 8:19 AMnew subject after splitting Last edited by: JD_techmania at: 3/6/2011 9:48 AM |
|
3/8/2011 12:22 PM | |
Posts: 1776 Rating: (95)
|
Hi, why are you using WinCC V7.0 SP1? Use WinCC V7.0 SP2. This is released for Windows Server 2008. See the compatibility list with the link http://support.automation.siemens.com/WW/view/en/21927773 A free of charge download of the WinCC V7.0 SP2 you can get with the link: http://support.automation.siemens.com/WW/view/en/44452271 |
3/9/2011 9:13 AM | |
Posts: 134 Rating: (11) |
You are lucky that you have this problem now, when there is WCC 7 sp2 |
3/27/2011 12:51 PM | |
Posts: 134 Rating: (11) |
Try to install it with Administrator account. Maybe activate windows first? |
3/29/2011 1:31 PM | |
Posts: 95 Rating: (1) |
Hi Janac, We installed it in Administrator account but still no success. JD |
3/29/2011 1:36 PM | |
Posts: 799 Rating: (43)
|
Hi, maybe you should try this: How should you proceed if installation of the Microsoft SQL server fails? regards |
5/11/2011 12:06 PM | |
Posts: 95 Rating: (1) |
Hi All, We areinstalling Server Client Configuration in our project. It has... 1)2 Dell Power Edge R510 Servers. 2)4 OS 3)1 ES. SERVERS In Servers we have installed 1)Windows Server 2008 SP2 (first we installed Windows Server 2008 from WindowsCD and than we upgraded it from microsoft website) 2)WinCC V7.0 SP2 ( which we downloaded from Siemens Linkhttps://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=44452271&caller=view) 3)It is communicating to our system via CP1623 card (one on each Server ) configured in Netpro. CLIENTS In Clients we have 1)Windows XP 2)WinCC V7.0 SP1 3)It is communicating to our system via TCP/IP inbuilt card. theproblem(or Towards a SOLUTION) 1) We have made a Multi User WinCC project with tags in Named Connection in Server and have genertaed its Server Data.It is communicating to our H systemwith temporary connection lost for few seconds. 2) When we go for "INTERCONNECT" option in Simatic Shell of client, WinCC opensand gives following error " Error in Aso wrapper, GetASO call ",but we are able to "disable" Server Porject from client. 3)After that we made a blank Client project in WinCC imported Server .pck file into it andwent online ->got following error "Do not have right to access WinCC project" ,now when we closed WinCC and again opened it-> the play button is disabled and stop buttton is enabled as it happens, in case, when WinCC is in Runtime, but now it does not show an Runtime Project running. It may be multiple problems comming in loads or may be a small glitch which we are missing. Weknow we will overcome it from our experts suggestions....waiting for them, hope we will make it. Regards, JD |
Last edited by: JD_techmania at: 5/11/2011 12:11 PM |
|
5/21/2011 7:07 AM | |
Posts: 95 Rating: (1) |
Hi all, can anybody help me on this.?? |
5/23/2011 7:18 AM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
"Do not have right to access WinCC project" For this, you should check user rights and make sure that they belong to the right user group(s) |
B r g d s , |
|
Follow us on