Industry Online Support
Technical Forum
4/22/2013 7:51 AM | |
Joined: 3/14/2008 Last visit: 6/27/2024 Posts: 2075 Rating: (930) |
Hello, We have one OSS that is configured with windows server 2003 and we have a new OSS but preinstalled is windows server 2003 R2. Is there a problem with PCS7 6.1 SP4 and using the two operating systems in a redundancy set up? |
If I could help you, you can use the RATE button. Thank you. |
|
4/23/2013 10:27 AM | |
Posts: 140 Rating: (7) |
Hi, As per my knowledge, i think we can use two different OS, But recommended to use same OS in both the servers. |
Follow us on