11/15/2011 6:18 AM | |
Posts: 98 Rating:
|
Hi Ganes, So how about with the Step 7, no need again.? शुक्रिया Cheers. Ando
|
11/15/2011 7:35 AM | |
Joined: 8/31/2010 Last visit: 7/15/2024 Posts: 1519 Rating:
|
I can't get you, can you put it with some other words? |
Like it? Rate it! |
|
11/15/2011 9:25 AM | |
Posts: 98 Rating:
|
|
11/15/2011 9:58 AM | |
Joined: 8/31/2010 Last visit: 7/15/2024 Posts: 1519 Rating:
|
TIA Portal v11 STEP 7 STEP 7 (TIA Portal) is the engineering software for configuring the SIMATIC S7-1200, S7-300/400, and WinAC controller families. STEP 7 (TIA Portal) is available in 2 editions, depending on the configurable controller families: ● STEP 7 Basic for configuring the S7-1200 ● STEP 7 Professional for configuring S7-1200, S7-300/400, and WinACWinCC WinCC (TIA Portal) is an engineering software for configuring SIMATIC Panels, SIMATIC Industrial PCs, and Standard PCs with the WinCC Runtime Advanced or the SCADA System WinCC Runtime Professional visualization software. WinCC (TIA Portal) is available in 4 editions, depending on the configurable operator control systems: ● WinCC Basic for configuring Basic Panels WinCC Basic is included with every STEP 7 Basic and STEP 7 Professional product.
visualization software WinCC Runtime Advanced is a visualization software for PC-based single-station systems. WinCC Runtime Advanced can be purchased with licenses for 128, 512, 2k, 4k as well as 8k PowerTags (tags with a process interface).
SCADA System WinCC Runtime Professional WinCC Runtime Professional is a SCADA system for structuring a configuration ranging from single-station systems to multi-station systems including standard clients or web clients. WinCC Runtime Professional can be purchased with licenses for 128, 512, 2k, 4k, 8k, 64k, 102400, 153600 as well as 262144 PowerTags (tags with a process interface).
Advanced or WinCC Runtime Professional and HMI devices with SINUMERIK HMI Pro sl RT or SINUMERIK Operate WinCC RT Basic. |
Like it? Rate it! |
|
11/16/2011 2:23 AM | |
Posts: 98 Rating:
|
Hi Ganes, Thanks for Info, I will purpose phurcase this software. Cheers..
|
Follow us on