5/14/2009 8:23 AM | |
Posts: 2930 Rating:
|
Hi, on my unit if I disconnect the wire from the PT100 the value of the AI is 0. Even in the manual there is no wire brake detection noted. |
5/18/2009 6:24 PM | |
Posts: 2 Rating:
|
Thanks to you for your precious help |
12/5/2016 5:45 PM | |
Joined: 1/4/2016 Last visit: 6/30/2022 Posts: 5 Rating:
|
Hello, It is an old thread but I am facing the same issue. I tried to use the method described in the attached document, downloaded from here, to detect PT100 wire break with an AM2 RTD card. I downloaded the example on actual hardware but what happens is that there is no difference between short circuit or wire break. In both short & wire break, the card outputs 0 (raw) or -500 (scaled). Is it possible that the official example is wrong, or I am missing something. The only diffirence between the example and the hardware, is that my LOGO! is FS04. Attachmentwire_break_evaluation_pt100_pt1000_sensors_v8.pdf (106 Downloads) |
Follow us on