12/12/2011 1:53 PM | |
Posts: 3037 Rating: (192)
|
Hello, What doyou want todo exactly? Tweety |
12/14/2011 8:59 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi well i went through the documents for NAMUR I/P and found this manual, The link is as below 7TH00 Diagnostics Using the Process Image of Inputs IntroductionIn addition to the diagnostic messages by means of LED and module/DP diagnostics, the module 6ES7 321-7TH00-0AB0 also provides additional information on the validity of each input signal - the value status. The value status is stored in the process image as is the input signal. Value statusThe value status is additional binary information on a digital input signal. The value status is entered at the same time as the process signal in the process input image and provides information on the validity of the input signal. The value status is influenced by
Digital input and value status assignmentIn the process image, each input in the input word IW x of the module is assigned a value status in the subsequent IW x+2.
Meaning of value statusThe value status means:
Evaluation of the Value Status in PCS 7The value status is evaluated in your CFC program with block FC 277 "CH_DI: Digital Input". This module undertakes the processing of the digital input value of S7-300-Digital input modules. How the value status gets into the block:
If you use the driver wizard in PCS 7 (as of V 5.1), steps 2 and 3 are executed automatically by PCS 7. Information about FC 277 and Processing of the Input SignalsYou can find a detailed description of the block and how the input signals are processed in the PCS7 documentation. --------------------------------------------------- Further documents for all ET200M modules are avaliable in this link : ET200M modules I shall find out more for diagnostic function in NAMUR. Have fun... |
Jazz |
|
Follow us on