Industry Online Support
Technical Forum
12/22/2010 4:20 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi Greg, There is no standard solution to do this. The easiest way would be to check or there is communciation running between the IM151-8 and the CPU319 by a kind of a life bit you need to write by yourself. Another way could be to use SNMP a nice description/example is made in the following FAQ, you could try to create a similar design and read out the parameters in Scalance W747-1RR. Diagnosis and Monitoring of IWLANs using SNMP variables |
Best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on