1/27/2014 11:19 AM | |
Posts: 33 Rating: (0) |
Hi everyone, I've been trying to setup a wireless profibus-connection between two S7-400 station. We use 2 Westermo RM805 for the wireless radio link. When i configure the two stations as master-slave (DP-Protocol). Everything works fine. When i try to configure them as an S7-Connection, it doens't work. I've read on this forum /tf/WW/en/Posts/182 that anything besides the DP-Protocol is not possible. Now i would like to know why it is not possible. I've done some research but haven't found anything useful on the why part. Tnx in advance, Nico |
6/29/2015 4:37 PM | |
Posts: 1 Rating: (1) |
Were you able to find a solution to your wireless profibus problem? I have the same issue and looking for a solution |
6/29/2015 11:20 PM | |
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666) |
Hello, Just to add information to mes' post, you can find a presentation of the different DataEagle radio links from M2M in the following link: http://www.m2m-dynamics.com/products/m2m-wireless-com Hope this helps, Daniel Chartier |
Follow us on