Industry Online Support
Technical Forum
6/29/2011 8:53 AM | |
Posts: 3 Rating: (0) |
Hello, I'm going to wire the AM2 AQ module to my Logo!. It's the old version, the 6ED1055-1MM00-0BA0. I don't understand how to connect it. Could you please help me? On the upper part of module there are 2 of L+/M. I should connect only the first L+/M, isn't it? On lower part there are 2 rows of connections: 1st row is made of 4 connections: PE O O O O How to connect them? 2nd row is made of 4 connections: V1+ M1 and V2+ M2. Are these the analog outputs? Thanks a lot to everybody, Marco. |
6/29/2011 11:18 AM | |
Joined: 12/27/2006 Last visit: 5/23/2024 Posts: 1196 Rating: (113) |
If you use a 0 (2) - 10 Volt signal, its no problem 40 is much greater than 5 |
Follow us on