7/4/2013 7:12 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181)
|
Hello, Take a look atSIMATIC NET Twisted-Pair and Fiber-Optic Networks Search for"15-pin Sub-D" (on Chapter 4). There you will find description of the connection cable... Best regards, Hristo Mihalev
|
This contribution was helpful to1 thankful Users |
7/4/2013 7:24 AM | |||||
Joined: 9/27/2006 Last visit: 8/16/2024 Posts: 12277 Rating: (2680) |
Hello SolutionFinder; This 15-port connector is known as an AUI interface, and to connect an Ethernet CP using such an interface with a network you needed a special nterface block known as a transceiver. It acted as a media converter to the network.This is explained in the following manual: S7-CPs for Industrial Ethernet Configuring and Commissioning Manual Part A - General Application Annex A3 also has the pinout of the AUI 15-pin connector. I do not believe transceivers are available any morefor a RJ-45 connection. Butour friendJ_Bell proposes an alternative in the following thread: DTE AUI port to Ethernet converter
Hope this helps,
|
||||
This contribution was helpful to1 thankful Users |
7/4/2013 8:13 AM | |
Posts: 559 Rating: (87) |
Dear dchartier & UMENCHO, Thanks for your fast response. But I want to communicate the same with PC through Ethernet only. I want to use wincc flexible runtime & to communicate PLC through this module CP 443-1 as mentioned above & for that I have made cable as UMENCHO has given the manual from the page no 4-31 i) Pinning of the TP XP Cord 15/RJ-45 Will it work? |
7/4/2013 9:02 AM | |
Posts: 559 Rating: (87) |
Thanks a lot. I will check & revert back. |
This contribution was helpful to1 thankful Users |
11/28/2019 2:51 PM | |
Posts: 9 Rating: (1) |
Hello , I have the same problem as you, can you send me the schema of your cabllage between the RJ45 and the subD15 Thank you
|
2/3/2020 12:26 AM | |
Posts: 9 Rating: (1) |
Hi Noodles, thank you for your answer ! The problem is resolved, i used a convertissor to communicate with the computer in real time. Bests Regards, Saidi S. |
Follow us on