4/20/2021 1:32 PM | |
Joined: 8/12/2016 Last visit: 5/21/2024 Posts: 101 Rating: (3) |
Dear Siwarexi, I am creating my project and written all my functions. I want to add the siwarex wp231 function to my project. I used the library provided through this link "https://support.industry.siemens.com/cs/ww/en/view/66825585" But when compiling the project it gives the following error: Network 15,Block "WP231PR_DB" that is accessed has not been compiled Network 15,Block "WP231PR" that is accessed has not been compiled And when I try to compile the WP231PR function it is not succeeded and gives this error: WP231PR (FB231),The block can only be compiled with a valid password. What is the solution for that? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/21/2021 07:15:19Optimized link. Last edited by: Jen_Moderator at: 04/21/2021 07:18:53New subject after splitting |
|
This contribution was helpful to1 thankful Users |
4/20/2021 2:21 PM | |
Joined: 8/12/2016 Last visit: 5/21/2024 Posts: 101 Rating: (3) |
I use the KTP700 for visulization, but even before downloading, I am having an error as I mentioned. I found the library in the link under the following zip folder ready_for_use_s7.zip (87,7 MB) |
Last edited by: msgsadek at: 04/20/2021 14:25:59 |
|
4/20/2021 2:34 PM | |
Joined: 9/12/2020 Last visit: 3/28/2024 Posts: 22 Rating: (0) |
wich plc do you use ? |
4/20/2021 2:36 PM | |
Joined: 8/12/2016 Last visit: 5/21/2024 Posts: 101 Rating: (3) |
1214 AC/DC/Rly 6ES7 214-1BG31-0XB0 |
4/20/2021 3:01 PM | |
Joined: 8/12/2016 Last visit: 5/21/2024 Posts: 101 Rating: (3) |
I tried the library and tried to copy from the ready used program but I am having error |
Follow us on