Industry Online Support
Technical Forum
9/11/2011 8:52 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, The idea is to use SFC46 (Puts the CPU into STOP mode and thus ends program processing). Press F1 in order to use in built help in Step7. Use a positive edge in order to start the timer (again use a F1 help in order to understand which type of timer is needing there). About retentive memory and S7-300 take a look at http://support.automation.siemens.com/WW/view/en/598803 Best regards, Hristo Mihalev |
Follow us on