6/25/2019 1:35 PM | |
Joined: 7/25/2017 Last visit: 9/19/2024 Posts: 317 Rating: (47) |
I've trawled through the documentation and the Internet, and maybe I'm missing something obvious, but I can't get any more info on the following problem. This is for a plug and play driver for V90s. -V90 is reset to factory defaults. -Add the V90 as a GSD device in TIA Portal with Telegram 111 -Using SINA_PARA_S, I can read P922 (its value is 105.0), but I can't write to it. -Values are Error=False, ErrorNo=2, ErrorID=1 - the drive rejects writing to this parameter - okay - but where is the info on ErrorNo=2? Some Siemens documentation leads to this document, but it is behind a membership wall:https://www.profibus.com/download/profidrive-profile-drive-technology/ AttachmentV90 SINA_PARA_S.zip (273 Downloads) |
6/28/2019 6:44 AM | |
Joined: 7/25/2017 Last visit: 9/19/2024 Posts: 317 Rating: (47) |
Siemens technical support replied, the information is actually in the G120 fieldbus manual, chapter 3.2, page 47. https://support.industry.siemens.com/cs/ww/en/view/109757336 Attached for convenience. AttachmentG120_fieldbus_fct_man_0418_en-US - page 47-48.pdf (242 Downloads) |
Follow us on